何をお探しですか?
Keysight Demonstrates 6G Neural Receiver Design Flow in Collaboration with NVIDIA at Mobile World Congress 2024
- Demonstration of neural receiver performance inside an Open RAN testbed
- Tools for complete design flow include ability to train the neural receiver using site-specific scenarios
- External channel models simulated by NVIDIA Sionna are emulated using Keysight equipment to create custom end-to-end system
SANTA ROSA, Calif. February 16, 2024
Keysight Technologies, Inc. (NYSE: KEYS) has collaborated with NVIDIA to create a complete design flow for training and validating neural receivers that will be shown at Mobile World Congress Barcelona 2024. To be presented at Keysight's booth, Hall 5 Stand 5E12, the demonstration will feature an Open RAN testbed that has been augmented by a multi-user MIMO neural receiver.
While 5G integrates artificial intelligence (AI) to enhance specific components in wireless networks, 6G will be the first generation of wireless technology that is AI-native. A key goal is to develop site-specific neural receivers to replace the entire human-designed receive chain of the physical layer. Yet, the data required to train these neural receivers is limited, and validating their performance in end-to-end systems presents a challenge. Before neural receivers can be deployed in commercial networks, they need to be adequately trained, demonstrated to surpass traditional receivers in performance and shown to robustly handle the channel conditions of real-world networks.
This demonstration shows how Keysight solutions enable the design and validation of a neural receiver. With the NVIDIA Sionna library used to train the neural receiver, ray-traced channels allow for site-specific training data generation and hence the creation of digital twins of real-world systems. As such, the neural receiver can be optimized for any intended environment.
When the training is complete, the neural receiver is deployed in an Open RAN testbed using Keysight's equipment connected to a FlexFi commercial radio unit from LITEON Technology. To emulate the site-specific channel, the Keysight PROPSIM channel emulator is used. It allows for the seamless import of ray-traced channel impulse responses. The trained neural receiver then demodulates the signal. Measurements of the block error rate of the end-to-end system provide insights into the neural receiver's performance.
Giampaolo Tardioli, Vice President, 6G and Next Generation Technology at Keysight, said: "By collaborating with industry leaders like NVIDIA, Keysight is helping provide the tools and insights needed to allow artificial intelligence to move into the mainstream for wireless communications. Through use of our simulated and measured data for training digital twins of Open RAN networks and the validation of AI performance, we are able to provide the complete end-to-end design environment that is needed to develop neural receivers and other AI components for 6G."
Ronnie Vasishta, Senior Vice President of Telecom at NVIDIA, said: "Software-defined RAN enables the native integration of AI across the entire protocol stack, ultimately leading to 6G systems that can optimally adapt to any environment. Keysight's ability to generate and capture real-world data for training and evaluation, bolstered by the open-source NVIDIA Sionna library for 6G physical-layer research, is a key element helping to drive the adoption of AI in wireless networks."
This demonstration includes technology that was developed as part of CENTRIC and 6G-SANDBOX, projects that have received funding from the Smart Networks and Services Joint Undertaking (SNS JU) under the European Union's Horizon Europe research and innovation program under Grant Agreement No 101096379 & 101096328, respectively.
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
Paul Erwin, Americas
+1 248 430–9075
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Jenny Gallacher, Europe
+44 (0) 7800 737–982
[email protected]
Need to contact Media Relations at Keysight?