데이터 시트
For Keysight InfiniiVision X-Series Oscilloscopes
Learn How to Perform Frequency Response Analysis Measurements
The DSOXBODE Bode plot training kit can be used to train engineering students and other oscilloscope users on how to perform frequency response analysis measurements (gain & phase Bode plots) using Keysight’s InfiniiVision oscilloscopes with the built-in WaveGen function generator. It includes a small training board consisting of a series R-L-C circuit with a BNC input that attaches directly to the output of the oscilloscope’s WaveGen function generator. There are clearly labeled test points for probing VIN and BPFOUT (bandpass filter output) or LPFOUT (low-pass filter output).
Also included with this training kit is a comprehensive tutorial and lab guide that engineering students and professors can download at www.keysight.com/find/bode. This training guide begins with a tutorial on frequency response measurements with fill-in-the-blank questions, and then provides step-by-step lab instructions on how to perform Bode plots measurements — both manually and automatically — using Keysight InfiniiVision oscilloscopes. The screen image below shows a gain & phase versus frequency test on the bandpass filter output of the DSOXBODE using a DSOX1204G InfiniiVision oscilloscope.
The DSOXBODE Bode plot training kit is compatible with InfiniiVision XSeries “G” model oscilloscopes and all InfiniiVision 3000T, 4000A, and 6000A X-Series oscilloscopes licensed with any software option.
무엇을 찾고 있습니까?