何をお探しですか?
Media Advisory
Keysight to Demonstrate Solutions Designed to Accelerate Innovation at electronica 2024
SANTA ROSA, Calif. October 29, 2024
What: At electronica 2024, Keysight Technologies will showcase a range of solutions designed to accelerate innovations in electronic design and test. Demonstrations will include the new HD3 oscilloscope and the PNA-X vector network analyzer. In addition, Keysight will showcase innovations in RF, digital, power testing, and the latest developments in PathWave Design electronic design automation (EDA) software.
When: November 12-15, 2024
Where: Keysight booth: Hall A3, stand 506; Trade Fair Center, Messe München in Munich, Germany
Media: Contact Jenny Gallacher to schedule media briefings and solution demonstrations.
Keysight will also hold an in-person media breakfast at electronica on Tuesday, November 12, at 9:00 a.m. CET. Interested journalists and industry analysts can contact Jenny Gallacher to reserve a spot.
Demonstrations include:
High-Speed Digital Testing
- Debug with 14-bit Resolution: Keysight will demo the new InfiniiVision HD3 series, a 14-bit analog-to-digital converter (ADC) oscilloscope, delivering four times the signal resolution and half the noise floor of other general-purpose oscilloscopes. Newly designed and built from the ground up with a custom application-specific integrated circuit (ASIC) and deep memory architecture, the HD3 Series enables engineers to quickly detect and fix signal issues in a variety of applications.
Network Analyzers
- Simplified Converter Test: The newly launched PNA-X vector network analyzer will be on display. This highly configurable instrument features four radio frequency (RF) signal sources, two internal combiners, and two low-noise receivers that accelerate component characterization.
- Precision RF Field and Lab Test: Keysight will demonstrate its FieldFox handheld analyzer, which is equipped to handle the toughest conditions and deliver precision measurements.
Connected Vehicles
- Validate Vehicle Networks: As modern vehicles integrate technologies, Keysight will showcase how to design, debug and analyze these complex systems with its oscilloscope portfolio. These support triggering and decoding of 10BASE-T1S, 100BASE-T1, and 1000BASE-T1 automotive ethernet standards and are compatible with over 50 protocols. Keysight will also demonstrate for the first time the successful test of forward and reverse transmit eye mask with a GMSL2 camera device with the Keysight UXR oscilloscope.
Power and Bench Measurements
- Next-Generation Bench Solutions: This will feature Keysight’s bench solutions which are designed to provide the broadest range of source and measurement solutions, from dependable TrueVolt digital multimeter to compact multi-channel power suppliers. In addition, the new portable RF and microwave analog signal generators will be on display.
Accelerating Design and Automating Intelligence
- Shift Left with EDA Software: The latest developments in Keysight’s Advanced Design System (ADS), the flagship product of its electronic design automation software, will be showcased. ADS enables shorter design cycles and first-pass design success for RF and microwave and high-speed digital printed circuit boards. Automating Intelligence is Keysight’s software model that provides deep insights and workflow automation for organizations.
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product life cycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
North America PR Team
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Jenny Gallacher, Europe
+44 (0) 7800 737–982
[email protected]