何をお探しですか?
Keysight Enables Open RAN Massive MIMO Innovation
- Solution optimizes the performance of Intel PSG’s complex massive MIMO beamforming technology
- Accelerates adoption of Open RAN network architectures by validating Intel PSG’s massive MIMO beamforming technology
SANTA ROSA, Calif. February 26, 2024
Keysight Technologies, Inc. (NYSE: KEYS) is enabling Intel to develop and validate massive multiple-input, multiple-output (mMIMO) beamforming designs for use in Open Radio Access Networks (RAN) with Open RAN Studio, accelerating the adoption of Open RAN architectures by mobile network operators.
By separating software from hardware through open interfaces and virtualization, Open RAN network architectures allow mobile operators to mix and match network elements from different vendors for increased flexibility and reduced costs. Operators can further improve network performance by implementing mMIMO, a technique of using large numbers of antennas to send and receive data to boost coverage and capacity. While Open RAN and mMIMO offer significant advantages, they also present significant conformance and interoperability challenges.
Implemented on a single Intel Agilex™ 7 system-on-chip field-programmable gate array (SoC FPGA), the Intel solution delivers efficient, high-quality signals through the antenna array using an Open RAN-compliant, weight-based dynamic beamforming method.
Intel ensured that its mMIMO digital beamforming solution could be seamlessly deployed in an Open RAN network by using the Keysight Open RAN Studio solution to validate its interoperability within the Open RAN ecosystem. Open RAN Studio enabled Intel to optimize the performance of its complex mMIMO beamforming technology to accommodate the large number of simultaneous connections needed to deliver the high data rates needed for 5G services.
Designed for LTE and 5G Open RAN Radio Unit (O-RU) testing, Open RAN Studio includes powerful Open RAN focused tools to construct, play, capture, and measure Open RAN traffic over Ethernet fronthaul interfaces. Open RAN Studio is part of the comprehensive Keysight Open RAN Architect (KORA) portfolio that provides test solutions for functional, performance, energy efficiency, security, and artificial intelligence and machine learning training and optimization.
Mike Fitton, Vice President and General Manger, Intel's Networking Business Division, said: "Keysight's support and robust equipment enables our engineering teams to develop and validate O-RAN compliant radios with a wide range of complex functionalities. Through our collaborative efforts, Intel and Keysight are empowering not only emerging but also established radio vendors to channel focus on core innovations in pursuit of providing vendor-agnostic O-RAN equipment within the dynamic landscape of 5G RAN."
Peng Cao, Vice President and General Manager, Keysight's Wireless Test Group, said: "Keysight continues to play an instrumental role in enabling the Open RAN ecosystem with its world-class test solutions. The successful validation of Open RAN mMIMO technology on Intel's solution is a significant step in the deployment of Open RAN networks. This milestone will help to accelerate the adoption of Open RAN network architectures by validating massive MIMO beamforming technology."
Resources
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
Paul Erwin, Americas
+1 248 430–9075
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Jenny Gallacher, Europe
+44 (0) 7800 737–982
[email protected]
Need to contact Media Relations at Keysight?