何をお探しですか?
Media Advisory
Keysight Spotlights Solutions Enabling Better AI Infrastructure at DesignCon 2024
SANTA ROSA, Calif. January 16, 2024
What: Keysight empowers innovators to accelerate the development of intelligent networks by pushing the boundaries of current data speeds. At DesignCon 2024, Keysight will demonstrate its market-leading design, simulation, and test solutions that enable electrical / optical transmission and data center interconnect applications to speeds of 800G and 1.6T.
When: January 30 – February 1, 2024
Where: Keysight Booth Number 1039
Santa Clara Convention Center
Media: Contact Paul Erwin to schedule media briefings and solution demonstrations.
Info: Keysight will present the following sessions at DesignCon 2024: Keysight Education Forum (KEF), technical presentations/papers, and more.
Join Keysight experts at Booth #1039 for the following demonstrations:
UCIe Chiplet PHY Designer – As AI workloads evolve and change, chiplet based system architectures can be used to scale up quickly to keep pace with the growing compute needs. This demo will showcase a new PHY designer for chiplets that allows the modeling, simulation, and analysis of the high-speed channel between two D2D PHY interfaces.
Enabling PCIe 7.0 Technology – PCIe architecture provides a robust high-bandwidth interconnect solution for attaching compute chips and network devices used in AI / ML applications. It also has the added benefit of a mature ecosystem that has been built up to include a compliance testing framework to ensure interoperability between different vendors. This will demonstrate Keysight's solutions that can be used to enable the testing of PCI Express 7.0 transmitter and receiver technologies.
PCIe 6.0 and CXL 2.0 Solutions – The rapid deployment of AI accelerators for use in compute arrays has driven the demand for higher speed PCIe chip-to-chip interfaces. Keysight's PCIe 6.0 Analyzer and PCIe 6.0 Exerciser solutions will be used to show how live PCIe 6.0 protocol traffic can be generated and analyzed using advanced triggers and filters while emulating both root complex and endpoint scenarios.
1.6T 212G PHY Transmitter/Receiver Testing – In order to process the large datasets associated with AI and large language models, bandwidth improvements are needed in both the compute-oriented interfaces as well as those used to enable higher speed data networks. Keysight will demonstrate the testing and validation of next-gen SerDes designs running at 212 Gbps per lane which are used to enable high-performance computing to unleash the potential of AI.
Test USB4 in Record Time – This demonstration spotlights Keysight's test solution for USB4 transmitter, receiver, and return loss as well as test automation software featuring measurement acceleration technology to provide the fastest time-to-answer in the market.
Signal Integrity PLTS 2024 – With an increase in demand for high-speed digital designs and interconnects aimed at enabling AI / ML applications, there are new signal integrity design and measurement challenges to consider. This demonstration will highlight vector network analysis and time domain reflectometry measurement solutions Keysight has developed to address these new challenges.
DDR5 Simulation and Test – AI / ML implementations impose challenging throughput demands on DRAM memory resources which has driven the adoption of DDR5 designs. Keysight will demonstrate a validation solution for DDR5 as well as a new high bandwidth and low noise probing solution which can be used to accurately report the Tx and Rx performance of next-gen memory designs.
PCI-SIG®, PCIe® and the PCI Express® are US registered trademarks and/or service marks of PCI-SIG.
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
Paul Erwin, Americas
+1 248 430–9075
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Jenny Gallacher, Europe
+44 (0) 7800 737–982
[email protected]
Need to contact Media Relations at Keysight?